Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MotionEnvironment.AdoptAssemblyJointStatus |
MotionEnvironment.AdoptAssemblyJointStatus.OFF
Adopt Assembly Joint is turned off
|
static MotionEnvironment.AdoptAssemblyJointStatus |
MotionEnvironment.AdoptAssemblyJointStatus.ON
Adopt Assembly Joint is turned on
|
static MotionEnvironment.AdoptAssemblyJointStatus |
MotionEnvironment.AdoptAssemblyJointStatus.UNDEFINED
Undefined status
|
Modifier and Type | Method and Description |
---|---|
MotionEnvironment.AdoptAssemblyJointStatus |
MotionEnvironment.getAdoptAssemblyJointStatus()
Gets the on-off status of adopt assembly joint
License requirements: mechanisms ("MECHANISMS") . |
static MotionEnvironment.AdoptAssemblyJointStatus |
MotionEnvironment.AdoptAssemblyJointStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MotionEnvironment.AdoptAssemblyJointStatus |
MotionEnvironment.AdoptAssemblyJointStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MotionEnvironment.AdoptAssemblyJointStatus[] |
MotionEnvironment.AdoptAssemblyJointStatus.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MotionEnvironment.setAdoptAssemblyJointStatus(MotionEnvironment.AdoptAssemblyJointStatus setting)
Sets the on-off status of adopt assembly joint
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.