Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PMDCMotorBuilder.Type |
PMDCMotorBuilder.Type.WITH_ROTOR
Included rotor - load torque
|
static PMDCMotorBuilder.Type |
PMDCMotorBuilder.Type.WITHOUT_ROTOR
Excluded rotor - rotor speed
|
Modifier and Type | Method and Description |
---|---|
PMDCMotorBuilder.Type |
PMDCMotorBuilder.motorType()
Returns the motor type
License requirements: nx_motion_motor ("NX Motion Motor") . |
static PMDCMotorBuilder.Type |
PMDCMotorBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PMDCMotorBuilder.Type |
PMDCMotorBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PMDCMotorBuilder.Type[] |
PMDCMotorBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PMDCMotorBuilder.setMotorType(PMDCMotorBuilder.Type motorType)
Sets the motor type
License requirements: nx_motion_motor ("NX Motion Motor") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.