public static class PMDCMotorBuilder.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_WITH_ROTOR
Included rotor - load torque
|
static int |
_WITHOUT_ROTOR
Excluded rotor - rotor speed
|
static PMDCMotorBuilder.Type |
WITH_ROTOR
Included rotor - load torque
|
static PMDCMotorBuilder.Type |
WITHOUT_ROTOR
Excluded rotor - rotor speed
|
Modifier and Type | Method and Description |
---|---|
static PMDCMotorBuilder.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PMDCMotorBuilder.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PMDCMotorBuilder.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final PMDCMotorBuilder.Type WITH_ROTOR
public static final PMDCMotorBuilder.Type WITHOUT_ROTOR
public static final int _WITH_ROTOR
public static final int _WITHOUT_ROTOR
public static PMDCMotorBuilder.Type valueOf(int value)
public static PMDCMotorBuilder.Type valueOf(String name)
public static PMDCMotorBuilder.Type[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.