Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
InputPortAssociation |
InputPortAssociationList.findItem(int index)
Returns the object at the input index.
|
InputPortAssociation[] |
InputPortAssociationList.getContents()
Gets the contents of the entire list
License requirements: None. |
InputPortAssociation |
MechatronicsBuilder.getInput(String inputName)
Retrieves an input port association from its name
License requirements: mechanisms ("MECHANISMS") . |
InputPortAssociation |
MechatronicsBuilder.newInputListItem()
Creates a new input list item including expressions
License requirements: mechanisms ("MECHANISMS") . |
Modifier and Type | Method and Description |
---|---|
void |
InputPortAssociationList.append(InputPortAssociation object)
Appends an object to the list
License requirements: None. |
void |
InputPortAssociationList.append(InputPortAssociation[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
InputPortAssociationList.erase(InputPortAssociation obj)
Erases the object from the list, but does not delete the object.
|
void |
InputPortAssociationList.erase(InputPortAssociation obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
InputPortAssociationList.findIndex(InputPortAssociation obj)
Finds the index where the input object appears.
|
void |
InputPortAssociationList.insert(int location,
InputPortAssociation object)
Inserts an object at the specified location
License requirements: None. |
void |
InputPortAssociationList.setContents(InputPortAssociation[] objects)
Sets the contents of the entire list.
|
void |
InputPortAssociationList.swap(InputPortAssociation object1,
InputPortAssociation object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.