Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.AmbientTempType.CONSTANT |
static TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.AmbientTempType.FUNCTION |
static TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.AmbientTempType.PROFILE |
static TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.AmbientTempType.TIRE_PARAMETER_FILE |
Modifier and Type | Method and Description |
---|---|
TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.ambientTempTypeSelection()
Returns the ambient temperature type.Specifies how the ambient temperature will be defined.
|
static TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.AmbientTempType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TirePropertyCdBuilder.AmbientTempType |
TirePropertyCdBuilder.AmbientTempType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TirePropertyCdBuilder.AmbientTempType[] |
TirePropertyCdBuilder.AmbientTempType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TirePropertyCdBuilder.setAmbientTempTypeSelection(TirePropertyCdBuilder.AmbientTempType ambientTempTypeSelection)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.