public static class TirePropertyCdBuilder.AmbientTempType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT |
static int |
_FUNCTION |
static int |
_PROFILE |
static int |
_TIRE_PARAMETER_FILE |
static TirePropertyCdBuilder.AmbientTempType |
CONSTANT |
static TirePropertyCdBuilder.AmbientTempType |
FUNCTION |
static TirePropertyCdBuilder.AmbientTempType |
PROFILE |
static TirePropertyCdBuilder.AmbientTempType |
TIRE_PARAMETER_FILE |
Modifier and Type | Method and Description |
---|---|
static TirePropertyCdBuilder.AmbientTempType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TirePropertyCdBuilder.AmbientTempType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TirePropertyCdBuilder.AmbientTempType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TirePropertyCdBuilder.AmbientTempType TIRE_PARAMETER_FILE
public static final TirePropertyCdBuilder.AmbientTempType CONSTANT
public static final TirePropertyCdBuilder.AmbientTempType FUNCTION
public static final TirePropertyCdBuilder.AmbientTempType PROFILE
public static final int _TIRE_PARAMETER_FILE
public static final int _CONSTANT
public static final int _FUNCTION
public static final int _PROFILE
public static TirePropertyCdBuilder.AmbientTempType valueOf(int value)
public static TirePropertyCdBuilder.AmbientTempType valueOf(String name)
public static TirePropertyCdBuilder.AmbientTempType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.