Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BushingDefine.ForceCalculationOption |
BushingDefine.ForceCalculationOption.ABC
ABC
|
static BushingDefine.ForceCalculationOption |
BushingDefine.ForceCalculationOption.BAB
BAB
|
static BushingDefine.ForceCalculationOption |
BushingDefine.ForceCalculationOption.STANDARD
Standard
|
Modifier and Type | Method and Description |
---|---|
BushingDefine.ForceCalculationOption |
BushingDefine.forceCalculation()
Returns the force calculation option
License requirements: mechanisms ("MECHANISMS") . |
static BushingDefine.ForceCalculationOption |
BushingDefine.ForceCalculationOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BushingDefine.ForceCalculationOption |
BushingDefine.ForceCalculationOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BushingDefine.ForceCalculationOption[] |
BushingDefine.ForceCalculationOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BushingDefine.setForceCalculation(BushingDefine.ForceCalculationOption opt)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.