Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MechatronicsBuilder.SolverCommunicationIntervalType |
MechatronicsBuilder.SolverCommunicationIntervalType.CONSTANT |
static MechatronicsBuilder.SolverCommunicationIntervalType |
MechatronicsBuilder.SolverCommunicationIntervalType.VARIABLE |
Modifier and Type | Method and Description |
---|---|
MechatronicsBuilder.SolverCommunicationIntervalType |
MechatronicsBuilder.communicationIntervalType()
Returns the communication interval type - possible values are Constant, Variable
License requirements: mechanisms ("MECHANISMS") . |
static MechatronicsBuilder.SolverCommunicationIntervalType |
MechatronicsBuilder.SolverCommunicationIntervalType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MechatronicsBuilder.SolverCommunicationIntervalType |
MechatronicsBuilder.SolverCommunicationIntervalType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MechatronicsBuilder.SolverCommunicationIntervalType[] |
MechatronicsBuilder.SolverCommunicationIntervalType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MechatronicsBuilder.setCommunicationIntervalType(MechatronicsBuilder.SolverCommunicationIntervalType communicationIntervalType)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.