Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static TirePropertyTnoBuilder.IswitchDefinitionType |
TirePropertyTnoBuilder.IswitchDefinitionType.DETAILED |
static TirePropertyTnoBuilder.IswitchDefinitionType |
TirePropertyTnoBuilder.IswitchDefinitionType.INTEGER |
Modifier and Type | Method and Description |
---|---|
TirePropertyTnoBuilder.IswitchDefinitionType |
TirePropertyTnoBuilder.iswitchDefinition()
Returns the iswitch definition.
|
static TirePropertyTnoBuilder.IswitchDefinitionType |
TirePropertyTnoBuilder.IswitchDefinitionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TirePropertyTnoBuilder.IswitchDefinitionType |
TirePropertyTnoBuilder.IswitchDefinitionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TirePropertyTnoBuilder.IswitchDefinitionType[] |
TirePropertyTnoBuilder.IswitchDefinitionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TirePropertyTnoBuilder.setIswitchDefinition(TirePropertyTnoBuilder.IswitchDefinitionType iswitchDef)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.