Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PackagingInterferenceBuilder.Action |
PackagingInterferenceBuilder.Action.CREATE_SOLIDS
Create solids of interference volumes.
|
static PackagingInterferenceBuilder.Action |
PackagingInterferenceBuilder.Action.HIGHLIGHT
Highlight interfering bodies.
|
static PackagingInterferenceBuilder.Action |
PackagingInterferenceBuilder.Action.SHOW_INTERSECTION_CURVE
Show intersection curve of interference volumes
|
Modifier and Type | Method and Description |
---|---|
PackagingInterferenceBuilder.Action |
PackagingInterferenceBuilder.actionType()
Returns the
PackagingInterference action type defined
at PackagingInterferenceBuilder.Action
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
static PackagingInterferenceBuilder.Action |
PackagingInterferenceBuilder.Action.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingInterferenceBuilder.Action |
PackagingInterferenceBuilder.Action.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingInterferenceBuilder.Action[] |
PackagingInterferenceBuilder.Action.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PackagingInterferenceBuilder.setActionType(PackagingInterferenceBuilder.Action aType)
Sets the
PackagingInterference action type defined
at PackagingInterferenceBuilder.Action
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.