public interface MotionMethods extends Remote
MotionMethods
class MotionSession
Modifier and Type | Method and Description |
---|---|
void |
copyConnectorParameters(NXObject sourceConnector,
NXObject destinationConnector)
Deprecated.
Deprecated in NX12.0.0. Use
copyParameters(nxopen.NXObject, nxopen.NXObject) instead.
|
void |
copyParameters(NXObject source,
NXObject destination)
Copy parameters from source to destination.
|
void |
exportParameters(NXObject entity,
String fileName)
Export parameters of an entity into a txt file.
|
void |
importParameters(NXObject entity,
String fileName)
Import parameters of an object into a txt file.
|
void |
modelCheck(boolean listWarning)
Check all motion objects
License requirements: mechanisms ("MECHANISMS") . |
void copyConnectorParameters(NXObject sourceConnector, NXObject destinationConnector) throws NXException, RemoteException
copyParameters(nxopen.NXObject, nxopen.NXObject)
instead.
sourceConnector
- Source connector from which parameters are copieddestinationConnector
- Destination connector to which the parameters are copied
NXException
RemoteException
void modelCheck(boolean listWarning) throws NXException, RemoteException
listWarning
- whether to display the checking result if only warnings found without errorNXException
RemoteException
void copyParameters(NXObject source, NXObject destination) throws NXException, RemoteException
source
- Source object from which parameters are copieddestination
- Destination object to which the parameters are copiedNXException
RemoteException
void exportParameters(NXObject entity, String fileName) throws NXException, RemoteException
entity
- entity to exportfileName
- file to export toNXException
RemoteException
void importParameters(NXObject entity, String fileName) throws NXException, RemoteException
entity
- entity to importfileName
- file to import fromNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.