Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AddSubmechanismBuilder.Layer |
AddSubmechanismBuilder.Layer.ORIGINAL
the original layer
|
static AddSubmechanismBuilder.Layer |
AddSubmechanismBuilder.Layer.SPECIFIED
custom specified layer
|
static AddSubmechanismBuilder.Layer |
AddSubmechanismBuilder.Layer.WORK
the work laye
|
Modifier and Type | Method and Description |
---|---|
AddSubmechanismBuilder.Layer |
AddSubmechanismBuilder.layerOption()
Returns the layers to which geometry are added
License requirements: None. |
static AddSubmechanismBuilder.Layer |
AddSubmechanismBuilder.Layer.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddSubmechanismBuilder.Layer |
AddSubmechanismBuilder.Layer.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddSubmechanismBuilder.Layer[] |
AddSubmechanismBuilder.Layer.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddSubmechanismBuilder.setLayerOption(AddSubmechanismBuilder.Layer layerOption)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.