public interface AddSubmechanismBuilder extends Builder, IAttributeSourceObjectBuilder
MotionSimulation.createAddSubmechanismBuilder(nxopen.NXObject)
Property | Value |
---|---|
LayerOption | Original |
UserLayer | 1 |
Modifier and Type | Interface and Description |
---|---|
static class |
AddSubmechanismBuilder.Layer
Represents initial location type that can be present during add component
|
Modifier and Type | Method and Description |
---|---|
AddSubmechanismBuilder.Layer |
layerOption()
Returns the layers to which geometry are added
License requirements: None. |
NXObject |
selectedPart()
Returns the Motion Simulation part to add as sumbechanism
License requirements: None. |
void |
setLayerOption(AddSubmechanismBuilder.Layer layerOption)
License requirements: mechanisms ("MECHANISMS") . |
void |
setSelectedPart(NXObject part)
License requirements: mechanisms ("MECHANISMS") . |
void |
setUserLayer(int layer)
License requirements: mechanisms ("MECHANISMS") . |
int |
userLayer()
Returns the user defined layer (should be a value in the range 1-256)
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
autoAssignAttributes, autoAssignAttributesWithNamingPattern, createAttributeTitleToNamingPatternMap
NXObject selectedPart() throws NXException, RemoteException
NXException
RemoteException
void setSelectedPart(NXObject part) throws NXException, RemoteException
part
- NXException
RemoteException
AddSubmechanismBuilder.Layer layerOption() throws NXException, RemoteException
NXException
RemoteException
void setLayerOption(AddSubmechanismBuilder.Layer layerOption) throws NXException, RemoteException
layerOption
- NXException
RemoteException
int userLayer() throws NXException, RemoteException
NXException
RemoteException
void setUserLayer(int layer) throws NXException, RemoteException
layer
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.