Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DriverOperation.Type |
DriverOperation.Type.ARTICULATION
Articulation
|
static DriverOperation.Type |
DriverOperation.Type.CONSTANT
Constant; Deprecated in NX11.0; use type_polynomial instead
|
static DriverOperation.Type |
DriverOperation.Type.CONTROL
Control
|
static DriverOperation.Type |
DriverOperation.Type.FUNCTION
Function
|
static DriverOperation.Type |
DriverOperation.Type.HARMONIC
Harmonic
|
static DriverOperation.Type |
DriverOperation.Type.MOTOR
Motor
|
static DriverOperation.Type |
DriverOperation.Type.POLYNOMIAL
Polynomial
|
static DriverOperation.Type |
DriverOperation.Type.PROFILE
Profile
|
static DriverOperation.Type |
DriverOperation.Type.UNDEFINED
Undefined
|
Modifier and Type | Method and Description |
---|---|
DriverOperation.Type |
DriverOperation.typeOption()
Returns the type option
License requirements: None. |
static DriverOperation.Type |
DriverOperation.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DriverOperation.Type |
DriverOperation.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DriverOperation.Type[] |
DriverOperation.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DriverOperation.setTypeOption(DriverOperation.Type typeOption)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.