Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.ACCELERATION
Acceleration
|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.DISPLACEMENT
Displacement
|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.FORCE
Force
|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.MOTOR_DRIVER
Motor Driver
|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.VELOCITY
Velocity
|
Modifier and Type | Method and Description |
---|---|
GraphBuilder.RequestChoices |
GraphBuilder.modeRequest()
Deprecated.
Deprecated in NX11.0.0. Use
GraphObjectBuilder instead.
|
GraphBuilder.RequestChoices |
GraphBuilder.request()
Deprecated.
Deprecated in NX11.0.0. Use
GraphObjectBuilder instead.
|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GraphBuilder.RequestChoices |
GraphBuilder.RequestChoices.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GraphBuilder.RequestChoices[] |
GraphBuilder.RequestChoices.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GraphBuilder.setModeRequest(GraphBuilder.RequestChoices modeRequest)
Deprecated.
Deprecated in NX11.0.0. Use
GraphObjectBuilder instead.
|
void |
GraphBuilder.setRequest(GraphBuilder.RequestChoices request)
Deprecated.
Deprecated in NX11.0.0. Use
GraphObjectBuilder instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.