Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CurveContactBuilder.GeometryMaterialSide |
CurveContactBuilder.GeometryMaterialSide.DIRECTION |
static CurveContactBuilder.GeometryMaterialSide |
CurveContactBuilder.GeometryMaterialSide.DIRECTION_REVERSE |
Modifier and Type | Method and Description |
---|---|
CurveContactBuilder.GeometryMaterialSide |
CurveContactBuilder.firstGeometryMaterialDirection()
Returns the first geometry materia side direction
License requirements: None. |
CurveContactBuilder.GeometryMaterialSide |
CurveContactBuilder.secondGeometryMaterialDirection()
Returns the second geometry materia side direction
License requirements: None. |
static CurveContactBuilder.GeometryMaterialSide |
CurveContactBuilder.GeometryMaterialSide.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveContactBuilder.GeometryMaterialSide |
CurveContactBuilder.GeometryMaterialSide.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveContactBuilder.GeometryMaterialSide[] |
CurveContactBuilder.GeometryMaterialSide.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CurveContactBuilder.setFirstGeometryMaterialDirection(CurveContactBuilder.GeometryMaterialSide sideDirection)
License requirements: mechanisms ("MECHANISMS") . |
void |
CurveContactBuilder.setSecondGeometryMaterialDirection(CurveContactBuilder.GeometryMaterialSide sideDirection)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.