Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
SignalChartListItem |
SignalChartCollection.createSignalChartListItem()
Creates a
SignalChartListItem
License requirements: nx_motion_motor ("NX Motion Motor") Created in NX6.0.0 |
SignalChartListItem |
SignalChartListItemList.findItem(int index)
Returns the object at the input index.
|
SignalChartListItem[] |
SignalChartListItemList.getContents()
Gets the contents of the entire list
License requirements: None. |
SignalChartListItem |
SignalChartBuilder.newListItemExpression(MotionSensor sensor,
boolean alwaysEvaluated,
int timeSensor,
int condition,
Expression threshold,
Expression delayTime,
Expression signal)
Creates a new list item including expression
License requirements: nx_motion_motor ("NX Motion Motor") . |
Modifier and Type | Method and Description |
---|---|
void |
SignalChartListItemList.append(SignalChartListItem object)
Appends an object to the list
License requirements: None. |
void |
SignalChartListItemList.append(SignalChartListItem[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SignalChartListItemList.erase(SignalChartListItem obj)
Erases the object from the list, but does not delete the object.
|
void |
SignalChartListItemList.erase(SignalChartListItem obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SignalChartListItemList.findIndex(SignalChartListItem obj)
Finds the index where the input object appears.
|
void |
SignalChartListItemList.insert(int location,
SignalChartListItem object)
Inserts an object at the specified location
License requirements: None. |
void |
SignalChartListItemList.setContents(SignalChartListItem[] objects)
Sets the contents of the entire list.
|
void |
SignalChartListItemList.swap(SignalChartListItem object1,
SignalChartListItem object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.