Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SignalChartListItem.Timer |
SignalChartListItem.Timer.ABSOLUTE_TIME
Absolute time
|
static SignalChartListItem.Timer |
SignalChartListItem.Timer.TIMER
Timer
|
static SignalChartListItem.Timer |
SignalChartListItem.Timer.UNDEFINED
Undefined, undefined timer for the sensor signal
|
Modifier and Type | Method and Description |
---|---|
SignalChartListItem.Timer |
SignalChartListItem.timeSensor()
Returns the time sensor
License requirements: nx_motion_motor ("NX Motion Motor") . |
static SignalChartListItem.Timer |
SignalChartListItem.Timer.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SignalChartListItem.Timer |
SignalChartListItem.Timer.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SignalChartListItem.Timer[] |
SignalChartListItem.Timer.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SignalChartListItem.setTimeSensor(SignalChartListItem.Timer timeSensor)
License requirements: nx_motion_motor ("NX Motion Motor") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.