Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PackagingMeasureBuilder.MeasureType |
PackagingMeasureBuilder.MeasureType.ANGLE
Measure angle between lines or linear edges.
|
static PackagingMeasureBuilder.MeasureType |
PackagingMeasureBuilder.MeasureType.MINIMUM_DISTANCE
Measure minimum distance between objects.
|
Modifier and Type | Method and Description |
---|---|
PackagingMeasureBuilder.MeasureType |
PackagingMeasureBuilder.msType()
Returns the Measure type defined at
PackagingMeasureBuilder.MeasureType
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
static PackagingMeasureBuilder.MeasureType |
PackagingMeasureBuilder.MeasureType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingMeasureBuilder.MeasureType |
PackagingMeasureBuilder.MeasureType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingMeasureBuilder.MeasureType[] |
PackagingMeasureBuilder.MeasureType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PackagingMeasureBuilder.setMsType(PackagingMeasureBuilder.MeasureType mType)
Sets the Measure type defined at
PackagingMeasureBuilder.MeasureType
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.