Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SignalChartBuilder.Type |
SignalChartBuilder.Type.CLOSED_LOOP
Closed loop
|
static SignalChartBuilder.Type |
SignalChartBuilder.Type.OPEN_LOOP
Open loop
|
Modifier and Type | Method and Description |
---|---|
SignalChartBuilder.Type |
SignalChartBuilder.signalChartType()
Returns the SignalChart type
License requirements: nx_motion_motor ("NX Motion Motor") . |
static SignalChartBuilder.Type |
SignalChartBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SignalChartBuilder.Type |
SignalChartBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SignalChartBuilder.Type[] |
SignalChartBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SignalChartBuilder.setSignalChartType(SignalChartBuilder.Type signalchartType)
Sets the SignalChart type
License requirements: nx_motion_motor ("NX Motion Motor") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.