Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MotionEnvironment.JointWizardStatus |
MotionEnvironment.JointWizardStatus.OFF
Joint Wizard is turned off
|
static MotionEnvironment.JointWizardStatus |
MotionEnvironment.JointWizardStatus.ON
Joint Wizard is turned on
|
static MotionEnvironment.JointWizardStatus |
MotionEnvironment.JointWizardStatus.UNDEFINED
Undefined status
|
Modifier and Type | Method and Description |
---|---|
MotionEnvironment.JointWizardStatus |
MotionEnvironment.getJointWizardStatus()
Gets the on-off status of joint wizard
License requirements: mechanisms ("MECHANISMS") . |
static MotionEnvironment.JointWizardStatus |
MotionEnvironment.JointWizardStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MotionEnvironment.JointWizardStatus |
MotionEnvironment.JointWizardStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MotionEnvironment.JointWizardStatus[] |
MotionEnvironment.JointWizardStatus.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MotionEnvironment.setJointWizardStatus(MotionEnvironment.JointWizardStatus setting)
Sets the on-off status of joint wizard
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.