Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BushingDefine.AngleCalculationOption |
BushingDefine.AngleCalculationOption.LARGE_ANGLE
Large Angle
|
static BushingDefine.AngleCalculationOption |
BushingDefine.AngleCalculationOption.SMALL_ANGLE
Small Angle
|
Modifier and Type | Method and Description |
---|---|
BushingDefine.AngleCalculationOption |
BushingDefine.angleCalculation()
Returns the angle calculation option
License requirements: mechanisms ("MECHANISMS") . |
static BushingDefine.AngleCalculationOption |
BushingDefine.AngleCalculationOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BushingDefine.AngleCalculationOption |
BushingDefine.AngleCalculationOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BushingDefine.AngleCalculationOption[] |
BushingDefine.AngleCalculationOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BushingDefine.setAngleCalculation(BushingDefine.AngleCalculationOption opt)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.