Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FlexBodyBuilder.SourceType |
FlexBodyBuilder.SourceType.LOCALFOLDER
File is in local folder
|
static FlexBodyBuilder.SourceType |
FlexBodyBuilder.SourceType.TEAMCENTER |
Modifier and Type | Method and Description |
---|---|
FlexBodyBuilder.SourceType |
FlexBodyBuilder.sourceOption()
Returns the file type
License requirements: None. |
static FlexBodyBuilder.SourceType |
FlexBodyBuilder.SourceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexBodyBuilder.SourceType |
FlexBodyBuilder.SourceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexBodyBuilder.SourceType[] |
FlexBodyBuilder.SourceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlexBodyBuilder.setSourceOption(FlexBodyBuilder.SourceType sourceOption)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.