Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PackagingInterferenceBuilder.Mode |
PackagingInterferenceBuilder.Mode.FACETED
Interference calculated by Faceted method.
|
static PackagingInterferenceBuilder.Mode |
PackagingInterferenceBuilder.Mode.PRECISE_SOLID
Interference calculated by Precise Solid method.
|
Modifier and Type | Method and Description |
---|---|
PackagingInterferenceBuilder.Mode |
PackagingInterferenceBuilder.modeType()
Returns the
PackagingInterference mode type defined
at PackagingInterferenceBuilder.Mode
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
static PackagingInterferenceBuilder.Mode |
PackagingInterferenceBuilder.Mode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingInterferenceBuilder.Mode |
PackagingInterferenceBuilder.Mode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingInterferenceBuilder.Mode[] |
PackagingInterferenceBuilder.Mode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PackagingInterferenceBuilder.setModeType(PackagingInterferenceBuilder.Mode mType)
Sets the
PackagingInterference mode type defined
at PackagingInterferenceBuilder.Mode
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.