Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
TirePropertyBasic
Basic Tire Property element. |
interface |
TirePropertyCd
CDTIRE Tire Property
This is an object that contains parameters needed for the CDTIRE Tire model
To create or edit an instance of this class, use TirePropertyCdBuilder Created in NX11.0.0 |
interface |
TirePropertyFt
FTire Tire Property element
This is an object that contains parameters needed for the FTire Tire model
To create or edit an instance of this class, use TirePropertyFtBuilder Created in NX11.0.0 |
interface |
TirePropertyMotorcycle
Motorcycle Tire Property element. |
interface |
TirePropertyNonInertial
NonInertial Tire Property element. |
interface |
TirePropertyTno
TNO Tire Property element
This is an object that contains parameters needed for the TNO Tire model
To create or edit an instance of this class, use TirePropertyTnoBuilder Created in NX11.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.