AddFontBuilder Class |
Builder for creating an add font user interface dialogue |
AlignStockBuilder Class |
Represents a Routing.AlignStockBuilder Builder for aligning non-circular stocks. |
Anchor Class |
A Routing Anchor defines a position in a Qualified Routing component part. |
AnchorCollection Class |
|
ArcSegment Class |
Represents a arc segment. |
ArcSegmentCollection Class |
Represents a collection of NXOpen.Routing.ArcSegment objects. |
AssemblyDefinition Class |
|
AssignCornerBuilder Class |
Builder class for Assign Corner which creates corner |
AssignDiscontinuityBuilder Class |
the Builder to Assign Discontinuity for the stocks |
AssignPathBuilder Class |
Assigns path to a broken routing run |
AttributeHolder Class |
Represents a NXOpen.Routing.AttributeHolder |
AttributeMembersBuilder Class |
Creates attibutemembers builder object to add to the search criteria list used by FindByAttributesBuilder |
BendCorner Class |
Computes a fillet curve between two linear segments to form a smooth bend transition from one segment to another. |
BendCornerCollection Class |
Represents a collection of NXOpen.Routing.BendCorner objects. |
BranchPathNumberingBuilder Class |
Builder class for Branch Path Numbering. |
BuiltInPath Class |
The Routing BuiltInPath object stores a set of curves. |
BuiltInPathCollection Class |
Represents a collection of NXOpen.Routing.BuiltInPath objects. |
CharacteristicList Class |
Contains a list of characteristics. |
ClockPartBuilder Class |
Builder class for clock part object |
CompareRunsBuilder Class |
Represents a NXOpen.Routing.CompareRunsBuilder , used to compare runs in the work part to the ones in another part, or to runs defined in xml files gathered in a folder (native mode) or on an item revision (managed mode). |
ConnectPathBuilder Class |
Represents a NXOpen.Routing.ConnectPathBuilder . |
ConnectedCurvesBuilder Class |
Builder for creating automatically creating segments on end-to-end connected curves. |
ConnectivityDefinition Class |
The base class for various connection objects.
|
ControlPoint Class |
Routing Control Points define a position in space, and are used to determine connections from segments to segments, and segments to ports. |
ControlPointCollection Class |
|
CopeCorner Class |
The cope corner is a corner that trims stocks at a junction. |
CopeCornerBuilder Class |
Builder class for Cope Corner object |
CopeCornerCollection Class |
Represents a collection of NXOpen.Routing.CopeCorner objects. |
Corner Class |
The Routing Corner is the abstract parent class of all other corner objects. |
CornerCollection Class |
Represents a collection of NXOpen.Routing.Corner objects. |
CornerTypeBuilder Class |
Contains setting for corner creation. |
CreateFabricationBuilder Class |
Builder class to fabricate subassembly from standard parts, path segments, stock, and other routing objects within the current routing assembly |
CrossSection Class |
A NXOpen.Routing.CrossSection defines a profile to sweep for NXOpen.Routing.Stock objects. |
CrossSectionCollection Class |
Represents a collection of NXOpen.Routing.CrossSection objects. |
DefineRunBuilder Class |
Builder Class for DefineRun Object |
DeleteFontsBuilder Class |
Represents a NXOpen.Routing.DeleteFontsBuilder |
DeleteGapsBuilder Class |
Represents a NXOpen.Routing.DeleteGapsBuilder |
DeleteObjectsBuilder Class |
Represents a NXOpen.Routing.DeleteObjectsBuilder |
DesignRule Class |
Represents NXOpen.Routing.DesignRule object |
DesignRuleCollection Class |
Represents a collection of NXOpen.Routing.DesignRule objects. |
DesignRuleManager Class |
Represents NXOpen.Routing.DesignRuleManager object |
DesignRuleOverride Class |
Represents Routing DesignRuleOverride object |
DesignRuleViolation Class |
Represents NXOpen.Routing.DesignRuleViolation object |
DesignRuleViolationCollection Class |
Represents a collection of NXOpen.Routing.DesignRuleViolation objects. |
DesignRuleViolationLocation Class |
Represents NXOpen.Routing.DesignRuleViolationLocation object |
DesignRuleViolationLocationCollection Class |
Represents a collection of NXOpen.Routing.DesignRuleViolationLocation objects. |
DesignRuleViolationViewer Class |
This class can be used to set the violation id, update text for overridding the violation and update the user name used to override the violation. |
DeviceRelationship Class |
|
DiscontinuityCorner Class |
A discontinuity corner is a corner that forces Routing.Stock objects to split as they cover the segments attached to the discontinuity corner. |
DiscontinuityCornerCollection Class |
Represents a collection of NXOpen.Routing.DiscontinuityCorner objects. |
Division Class |
Represents NXOpen.Routing.Division |
DivisionsBuilder Class |
Represents a NXOpen.Routing.DivisionsBuilder Builder for creating/editing splits at an end of a duct. |
DuctReinforcement Class |
Represents a Duct Reinforcement feature used for creating/editing reinforcements on the inside or outside of rectangular HVAC ducts. |
DuctReinforcementBuilder Class |
Builder for creating/editing duct reinforcements. |
DuctSizeCalculatorBuilder Class |
Builder to perform calculations of the duct which is to be used in the HVAC applications. |
EditBendAngleBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.Routing.RouteManager.CreateEditBendAngleBuilder`</para> |
EditCharacteristicsBuilder Class |
Builder to edit required and optional characteristics of Routing.Stock or Assemblies.Component as defined in the application view file. |
EditLineSegmentBuilder Class |
Builder for the Edit Line Segment operation. |
EditPlacePartBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.Routing.RouteManager.CreateEditPlacePartBuilder`</para> |
ElbowSnapSettings Class |
Helper object used the by NXOpen.Routing.LinearPathBuilder builder. |
ExtractPort Class |
Routing ExtractPort object is an extract of Port class |
FeaturePort Class |
NXOpen.Routing.FeaturePort is a NXOpen.Features.Feature associated with NXOpen.Routing.Port . |
Filler Class |
Represents a Filler |
FillerCollection Class |
Represents a collection of NXOpen.Routing.Stock objects. |
FillerStockBuilder Class |
Creates Filler stock on selected Segments. |
FindByAttributesBuilder Class |
Find runs/objects with specified attribute name and attribute value criteria, highlight the corresponding nodes in the run navigator and the graphics area |
FittingOverstock Class |
The NXOpen.Routing.FittingOverstock object represents overstock applied over the faces of the routing parts. |
FittingOverstockBuilder Class |
Builder for creating or editing NXOpen.Routing.FittingOverstock objects. |
FittingOverstockCollection Class |
Represents a collection of NXOpen.Routing.FittingOverstock objects. |
FittingPort Class |
Represents a Routing Fitting Port Object:py:class:NXOpen.Routing.FittingPort. |
FittingPortCollection Class |
Represents a collection of NXOpen.Routing.FittingPort objects. |
FixturePort Class |
NXOpen.Routing.FixturePort objects are objects that * segments are routed through when creating a routing path. |
FixturePortCollection Class |
Represents a collection of NXOpen.Routing.FixturePort objects. |
FormboardFrame Class |
The NXOpen.Routing.FormboardFrame is a (not pure) virtual class. |
FormboardFrameCGM Class |
Represents a Formboard Frame CGM. |
FormboardFrameCollection Class |
Represents a collection of NXOpen.Routing.FormboardFrame objects. |
FormboardFramePattern Class |
Represents a Formboard Frame Pattern. |
FormboardFrameRectangle Class |
Represents a Formboard Frame Rectangle. |
GapArcSegment Class |
Represents a gap arc segment. |
GapDisplayBuilder Class |
Builder for creating a gap arc object on a line segment. |
HandrailBuilder Class |
Represents a NXOpen.Routing.HandrailBuilder Creates a handrail from a selected point. |
HealPath Class |
Represents a NXOpen.Routing.HealPath object which holds the data used in the creation of the heal path spline. |
IAxisPort Class |
Interface class for all routing objects that specify a direction |
ICharacteristic Class |
Interface for querying and setting characteristic (UG attribute values) on various routing objects. |
IPath Class |
The Routing IPath object is a list of segments in a route. |
IRoutePosition Class |
Interface class for all routing objects that specify a single (possibly associative) location in space. |
ISegment Class |
Interface class for all routing segments [Line/Arc/Spline] |
ISegmentCollection Class |
Represents a collection of Routing.ISegment objects. |
InfoObjectsBuilder Class |
Represents a NXOpen.Routing.InfoObjectsBuilder |
InstanceNameLookupBuilder Class |
Represents a NXOpen.Routing.InstanceNameLookupBuilder . |
IntegrateRunsBuilder Class |
Builder Class for Integrate Runs Object |
InterfaceTerminalBase Class |
The NXOpen.Routing.InterfaceTerminalBase corresponds to an abstract class for a prototype NXOpen.Routing.Port . |
InterfaceTerminalRelationshipBase Class |
The abstract class NXOpen.Routing.InterfaceTerminalRelationshipBase relates many NXOpen.Routing.Port`s to one :py:class:`NXOpen.Routing.Port . |
InterfaceTerminalRelationshipCollection Class |
Represents a collection of NXOpen.Routing.InterfaceTerminalRelationshipShadow objects. |
InterfaceTerminalRelationshipShadow Class |
Represents an assembly shadow of NXOpen.Routing.InterfaceTerminalRelationshipBase . |
InterfaceTerminalShadow Class |
Represents the defining data for a physical NXOpen.Routing.Port . |
IsoDrawingBuilder Class |
Represents a NXOpen.Routing.IsoDrawingBuilder , used to run the ISOGEN engine to create isometric drawings of piping networks. |
ItemDefinition Class |
NXOpen.Routing.ItemDefinition object corresponds to DDID in AP212 and to a piece part or routing stock in NX. |
LineSegment Class |
Represents a line segment. |
LineSegmentCollection Class |
Represents a collection of NXOpen.Routing.LineSegment objects. |
LinearPathBuilder Class |
Builder for creating routing linear paths. |
LinearPathSettings Class |
Helper object used the by Routing.LinearPathBuilder builder. |
LogicalConnection Class |
Represents a connection between mutiple From and To Routing.LogicalTerminal .
|
LogicalTerminal Class |
Assembly instance of a NXOpen.Routing.InterfaceTerminalBase . |
ManualRouteBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.Routing.RouteManager.CreateManualRouteBuilder`</para> |
MergeStocksBuilder Class |
Represents a NXOpen.Routing.MergeStocksBuilder Builder for merging routing stocks ( including space reservation stocks ). |
MiterCorner Class |
This class defines a mitered corner. |
MiterCornerCollection Class |
Represents a collection of NXOpen.Routing.MiterCorner objects. |
MiteredBendCorner Class |
Computes a fillet curve between two linear segments to form a smooth bend transition from one segment to another that represents a mitered bend. |
MiteredBendCornerCollection Class |
Represents a collection of NXOpen.Routing.MiteredBendCorner objects. |
ModelTerminalsBuilder Class |
The Builder to Model/UnModel the Terminals |
MultiPort Class |
Represents a NXOpen.Routing.MultiPort . |
MultiPortCollection Class |
Represents a collection of NXOpen.Routing.MultiPort objects. |
ObjectRelationship Class |
Represents a relationship between Routing objects.
|
OffsetPath Class |
The Routing OffsetPath object is the set of information needed to define an offset route. |
OffsetPathCollection Class |
The Routing OffsetPath object is a list of segments in a route. |
Overstock Class |
Represents an NXOpen.Routing.Overstock object. |
OverstockApplication Class |
Represents a collection of NXOpen.Routing.OverstockApplication objects. |
OverstockApplicationCollection Class |
Represents a collection of NXOpen.Routing.OverstockApplication objects. |
OverstockBuilder Class |
Builder for creating/editing overstocks. |
OverstockFacesBuilder Class |
Builder for qualifying faces for overstock application over fittings. |
PartDefinitionBase Class |
The abstract class NXOpen.Routing.PartDefinitionBase contains information defining a logical part. |
PartDefinitionShadow Class |
NXOpen.Routing.PartDefinitionShadow contains the defining data for a logical part, such as an connector. |
Path Class |
The Routing Path object is the set of ordered continuous segments. |
PathStockBuilder Class |
Assigns stocks to segments based of users critiera and the current default stock. |
PlacePartBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.Routing.RouteManager.CreatePlacePartBuilderPTS`</para> |
PlacementSolutionsBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.Routing.RouteManager.CreatePlacementSolutionsBuilder`</para> |
Platform Class |
NXOpen.Routing.Platform objects are automatically created and updated by NXOpen.Routing.Platform objects. |
PlatformCreatorBuilder Class |
Builder for creating platform. |
PlatformFeature Class |
Represents a Platform feature. |
Port Class |
Routing Port Object is a parent class for FixturePort, ExtractPort, FittingPort, Multiport, StockPort and TerminalPort |
PortCollection Class |
|
PortConnection Class |
The Routing PortConnection object is used by Routing to position ports while placing parts. |
PortConnectionCollection Class |
Represents a collection of NXOpen.Routing.PortConnection objects. |
ProxyPort Class |
A NXOpen.Routing.ProxyPort is a port that represents a connector in another design zone, but not present in this design zone. |
ProxyPortCollection Class |
Represents a collection of NXOpen.Routing.ProxyPort objects. |
QuickPathBuilder Class |
Builder for creating a path between user selected points. |
RemoveDiscontinuityBuilder Class |
Builder class for remove discontinuity object |
ReuseLibrary Class |
Represents a NXOpen.Routing.ReuseLibrary |
RootObject Class |
The NXOpen.Routing.RootObject is the parent class of all other Routing logical objects. |
RouteLogicalAssociation Class |
RouteLogicalAssociation object associates non-electrical components to electrical components. |
RouteLogicalAssociationCollection Class |
Collection class for RouteLogicalAssociation object |
RouteManager Class |
Manages various Routing collections and methods for use in the current work part. |
RouteObject Class |
The Top level routing data model object.
|
RouteObjectCollector Class |
Represents a NXOpen.Routing.RouteObjectCollector class to create objects for getting routing objects. |
RoutePartDescriptor Class |
Represents a part descriptor chrx. |
RoutePartDescriptorCollection Class |
Represents a collection of NXOpen.Routing.RoutePartDescriptor objects. |
RouteSegmentFont Class |
Represents a route segment font. |
RouteSegmentFontElement Class |
Represents a route segment font element. |
RouteSweptFoldBuilder Class |
Represents a Rout Swept Fold Builder |
RouteSweptTwistBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.Routing.RouteManager.CreateRouteSweptTwistBuilder`</para> |
RoutingMeasureDistanceBuilder Class |
Represents a NXOpen.Routing.RoutingMeasureDistanceBuilder |
RoutingSystem Class |
Routing object is a collection of NXOpen.Routing.Run objects. |
RoutingSystemCollection Class |
Represents a collection of NXOpen.Routing.RoutingSystem objects. |
Run Class |
Routing Run object references components and stocks which comprise a piping run. |
RunCollection Class |
Represents a collection of NXOpen.Routing.Run objects. |
RunItem Class |
Routing Run Item object references components which comprise a piping run. |
RunItemsBuilder Class |
The builder for creating the list item of RunItems |
RunItemsBuilderList Class |
Represents a list of objects. |
SBendCorner Class |
The Routing SBendCorner defines a S-Bend. |
SBendCornerCollection Class |
Represents a collection of NXOpen.Routing.SBendCorner objects. |
SegmentManager Class |
Contains the type of the routing part as well as the Collection objects for creating/iterating over routing objects. |
SegmentPairBuilder Class |
The builder for creating the list item of SegmentPairs |
SelectControlPoint Class |
Represents a single object selection. |
SelectISegment Class |
Represents a single object selection. |
SelectLineSegment Class |
Represents a single object selection. |
SelectPort Class |
Represents a single object selection. |
SelectRun Class |
Represents a single object selection. |
SelectStock Class |
Represents a single object selection. |
SimplifyPathBuilder Class |
Represents a NXOpen.Routing.SimplifyPathBuilder for Simplify Path operation. |
SingleDevice Class |
The Routing SingleDevice corresponds to an abstract instance of NXOpen.Routing.ItemDefinition . |
SpaceReservationBuilder Class |
Represents a NXOpen.Routing.SpaceReservationBuilder This builder takes one or more segments and creates space reservation stock on it. |
SplinePathBuilder Class |
Builder for creating a D-Cubed constrained spline. |
SplineSegment Class |
Represents a spline segment. |
SplineSegmentCollection Class |
Represents a collection of NXOpen.Routing.SplineSegment objects. |
SplitDuctBuilder Class |
Represents a NXOpen.Routing.SplitDuctBuilder Builder for creating/editing splits at an end of a duct. |
SplitRunBuilder Class |
Builder Class for Split Run Object |
Stock Class |
The NXOpen.Routing.Stock object represents a material (such as as pipe or tube) that covers a path of segments. |
StockBrowserBuilder Class |
Builder class for stock browser . |
StockBuilder Class |
Builder for creating/editing stocks. |
StockCollection Class |
Represents a collection of NXOpen.Routing.Stock objects. |
StockColorBuilder Class |
Represents a NXOpen.Routing.StockColorBuilder . |
StockData Class |
A NXOpen.Routing.StockData contains the various profiles, characteristic information, NXOpen.Routing.Anchor and other attributes that define NXOpen.Routing.Stock objects. |
StockDataCollection Class |
Represents a collection of NXOpen.Routing.StockData objects. |
StockDefinition Class |
Represents Routing StockDefinition object |
StockDevice Class |
The Routing StockDevice corresponds to a generic stock instance of Routing.SingleDevice . |
StockOffsetPointBuilder Class |
Applies Assemblies Constraints to a selected NXOpen.Point or NXOpen.Routing.ControlPoint to mimic the update/move behavior of the input smart NXOpen.Point . |
StockOffsetPort Class |
NXOpen.Routing.StockOffsetPort class handles the relationship between a component part’s port occurrence and the dumb offset port in the work part. |
StockOffsetPortCollection Class |
Represents a collection of NXOpen.Routing.StockOffsetPort objects. |
StockPartConverterBuilder Class |
Represents a NXOpen.Routing.StockPartConverterBuilder Builder for Part Conversion of the stocks. |
StockPort Class |
NXOpen.Routing.StockPort objects are automatically created and updated by NXOpen.Routing.Stock objects. |
StockStyleBuilder Class |
Builder class to assigns style to the selected stock . |
StockTransition Class |
Represents NXOpen.Routing.StockTransition object. |
StockTransitionBuilder Class |
Builder for creating/editing stockTransition. |
SubdivideSegmentBuilder Class |
Represents a NXOpen.Routing.SubdivideSegmentBuilder . |
TerminalPort Class |
A NXOpen.Routing.TerminalPort models the pins on an electrical connector. |
TerminalPortBuilder Class |
Builder for creating the Terminal List Item for the ModelTerminals |
TerminalPortCollection Class |
The collection of all :py:class:`NXOpen.Routing.TerminalPort`s. |
TransformPathBuilder Class |
Builder for the Transform Path operation. |
UnifyPathBuilder Class |
Builder to unify Routing.Stock and Assemblies.Component based on specified characteristic values. |
WatertightFittingsBuilder Class |
Represents a NXOpen.Routing.WatertightFittingsBuilder |
WindCatcher Class |
Represents a Wind Catcher feature. |
WindCatcherBuilder Class |
Builder class for Wind Catcher feature. |
Wire Class |
The Routing Wire object is the set of information needed to define * a ROUTE_wire. |
WireCollection Class |
The Routing Wire object is a list of segments in a route and some stock. |