StockStyleBuilder Class¶
-
class
NXOpen.Routing.
StockStyleBuilder
¶ Bases:
NXOpen.Builder
Builder class to assigns style to the selected stock .
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateStockStyleBuilder()
Default values.
Property Value EnumStockStyle SimpleSolid New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
EnumStockStyle | Returns or sets the enum for setting stock style |
RouteSelectionStock | Returns the route selection stock for selecting routing objects |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StockStyleBuilderStockStyle Enumeration | Enum to define the stock style |
Property Detail¶
EnumStockStyle¶
-
StockStyleBuilder.
EnumStockStyle
¶ Returns or sets the enum for setting stock style
-------------------------------------
Getter Method
Signature
EnumStockStyle()
Returns: Return type: NXOpen.Routing.StockStyleBuilderStockStyle
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
EnumStockStyle(enumStockStyle)
Parameters: enumStockStyle ( NXOpen.Routing.StockStyleBuilderStockStyle
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RouteSelectionStock¶
-
StockStyleBuilder.
RouteSelectionStock
¶ Returns the route selection stock for selecting routing objects
-------------------------------------
Getter Method
Signature
RouteSelectionStock()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
StockStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.