RunStatus Enumeration¶
NXOpen.Routing.Run.Status is an alias for NXOpen.Routing.RunStatus
-
class
NXOpen.Routing.
RunStatus
¶ Bases:
object
Represents the status of a run
Enum Members
- stocks assigned on them “
- “Broken”, ” Run is broken. All items are not connected end to end ” “Incomplete”, ” Run is incomplete. Some segments do not have stock assigned on them”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.