BendCornerCollectionType Enumeration¶
NXOpen.Routing.BendCornerCollection.Type is an alias for NXOpen.Routing.BendCornerCollectionType
-
class
NXOpen.Routing.
BendCornerCollectionType
¶ Bases:
object
Option for creating a bend using a bend table or using radius or ratio
Enum Members
- create a bend corner. “
- “Table”, ” Using a bend table to create a
bend corner. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.