TerminalPortBuilder Class¶
-
class
NXOpen.Routing.
TerminalPortBuilder
¶ Bases:
NXOpen.Builder
Builder for creating the Terminal List Item for the ModelTerminals
To create a new instance of this class, use
NXOpen.Routing.RouteManager.TerminalPortBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
IndividualCutBack | Returns the Cutback Lenth for the Terminal |
IndividualExtenstion | Returns the Extenstion Value for the Terminal |
Modeled | Returns or sets the flag for the terminal that says if it is Modeled or not |
Tag | Returns the Tag for this object. |
TerminalPort | Returns or sets the TerminalPort |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IndividualCutBack¶
-
TerminalPortBuilder.
IndividualCutBack
¶ Returns the Cutback Lenth for the Terminal
-------------------------------------
Getter Method
Signature
IndividualCutBack()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
IndividualExtenstion¶
-
TerminalPortBuilder.
IndividualExtenstion
¶ Returns the Extenstion Value for the Terminal
-------------------------------------
Getter Method
Signature
IndividualExtenstion()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Modeled¶
-
TerminalPortBuilder.
Modeled
¶ Returns or sets the flag for the terminal that says if it is Modeled or not
-------------------------------------
Getter Method
Signature
Modeled()
Returns: Return type: bool New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
Modeled(modeled)
Parameters: modeled (bool) – New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
TerminalPort¶
-
TerminalPortBuilder.
TerminalPort
¶ Returns or sets the TerminalPort
-------------------------------------
Getter Method
Signature
TerminalPort()
Returns: Routing Port Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
TerminalPort(port)
Parameters: port ( NXOpen.NXObject
) – Routing PortNew in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
Validate¶
-
TerminalPortBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.