DesignRuleViolationBlankOption Enumeration

NXOpen.Routing.DesignRuleViolation.BlankOption is an alias for NXOpen.Routing.DesignRuleViolationBlankOption

class NXOpen.Routing.DesignRuleViolationBlankOption

Bases: object

Design Rule Violation Location Object Blank Option

Enum Members

Enum Member Enum Member Description
Blank  
Unblank
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.