SplineSegment Class¶
-
class
NXOpen.Routing.
SplineSegment
¶ Bases:
NXOpen.Spline
,NXOpen.Routing.ISegment
Represents a spline segment.
To obtain an instance of this class use
NXOpen.Routing.SplineSegmentCollection
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
FollowCurve | Returns the segment follow curve. |
IsBlanked | Returns the blank status of this object. |
IsFlexibleParametricSplineSegment | Returns a boolean value that indicates whether the spline has been converted to the new flexible parametric spline in NX9. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsReference | Returns the reference state of a curve |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
Length | Returns the length of the segment. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
Order | Returns the order of the spline |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Periodic | Returns the periodicity of the spline |
PoleCount | Returns the number of poles, includes the duplicates in case of periodic spline. |
Prototype | Returns the prototype of this object if it is an occurrence. |
Rational | Returns the rationality of the spline |
Tag | Returns the Tag for this object. |
Update | Returns the update option. |
Visibility | Returns the visibility. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
ConvertEccentricLinearToLinear | Is line segment eccentric converted to line segment? @return Is line segment eccentric converted to line segment? |
ConvertLinearToEccentricLinear | Is line segment converted to eccentric line segment? @return Is line segment converted to eccentric line segment? |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Evaluate | Evaluate a smart object. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Get3DPoles | Returns poles in three-dimensional cartesian coordinates of a normalized representation of the spline. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCableDevices | Returns NXOpen.Routing.Electrical.CableDevice objects from NXOpen.Routing.ISegment . |
GetCablewaysLayoutViews | Returns NXOpen.Routing.Electrical.CablewaysLayoutView objects from the NXOpen.Routing.ISegment . |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetDraftingCurveInfo | Creates new DraftingCurveInfo object @return New DraftingCurveInfo object. |
GetEndPoints | Get the current location of the segment ends in ABS coordinates. |
GetEndRcps | Return of segment end control points. |
GetGuid | Returns the Globally Unique Identifier (GUID) for this segment. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetIsEccentricSegment | Is given segment a eccentric segment? @return Is segment a eccentric segment? |
GetIsSegmentInterior | Query if a segment is interior to any part @return Is segment interior? |
GetIsTerminalSegment | Is given segment a terminal segment? @return Is segment a terminal segment? |
GetKnots | Returns the knots @return |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPoles | Returns the homogeneous poles. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSegmentAllStocks | Returns NXOpen.Routing.Stock as well as NXOpen.Routing.Overstock objects from the NXOpen.Routing.ISegment . |
GetSegmentStock | Returns all stocks that directly reference this segment as part of the path defining the stock. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveParameters | Removes the smart object parameters. |
RemoveViewDependency | Remove dependency on all views from an object. |
ReplaceParameters | Edit a smart object by replacing its parameters using parameters of other smart object of the same class. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristic2 | Sets or creates an integer type attribute associated with the input title. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetCharacteristics2 | Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already. |
SetEndPoints | Set the current location of the segment ends in ABS coordinates. |
SetEndRcps | |
SetIsTerminalSegment | Set given segment to be a terminal segment? |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSegmentInteriorPart | Set a segment to be interior to supplied part |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetVisibility | Sets the visibility. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
FollowCurve¶
-
SplineSegment.
FollowCurve
¶ Returns the segment follow curve.
NULL object indicates segment has no follow curve
-------------------------------------
Getter Method
Signature
FollowCurve()
Returns: Follow curve of segment Return type: NXOpen.Curve
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsFlexibleParametricSplineSegment¶
-
SplineSegment.
IsFlexibleParametricSplineSegment
¶ Returns a boolean value that indicates whether the spline has been converted to the new flexible parametric spline in NX9.
-------------------------------------
Getter Method
Signature
IsFlexibleParametricSplineSegment()
Returns: Is this a constrained spline? Return type: bool New in version NX9.0.3.
License requirements: routing_base (“Routing Basic”)
IsOccurrence¶
-
SplineSegment.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsReference¶
-
SplineSegment.
IsReference
¶ Returns the reference state of a curve
-------------------------------------
Getter Method
Signature
IsReference()
Returns: True - Reference; False - Not Reference Return type: bool New in version NX8.0.0.
License requirements: None.
JournalIdentifier¶
-
SplineSegment.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Length¶
-
SplineSegment.
Length
¶ Returns the length of the segment.
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: float New in version NX11.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Name¶
-
SplineSegment.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SplineSegment.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SplineSegment.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SplineSegment.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ConvertEccentricLinearToLinear¶
-
SplineSegment.
ConvertEccentricLinearToLinear
¶ Is line segment eccentric converted to line segment?
Signature
ConvertEccentricLinearToLinear()
Returns: Is line segment eccentric converted to line segment? Return type: NXOpen.Routing.ConvertEccentricLinearToLinear
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ConvertLinearToEccentricLinear¶
-
SplineSegment.
ConvertLinearToEccentricLinear
¶ Is line segment converted to eccentric line segment?
Signature
ConvertLinearToEccentricLinear()
Returns: Is line segment converted to eccentric line segment? Return type: NXOpen.Routing.ConvertLinearToEccentricLinear
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
DeleteCharacterstics¶
-
SplineSegment.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
SplineSegment.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCableDevices¶
-
SplineSegment.
GetCableDevices
¶ Returns
NXOpen.Routing.Electrical.CableDevice
objects fromNXOpen.Routing.ISegment
.Signature
GetCableDevices()
Returns: Array of cable devices. Return type: list of NXOpen.Routing.Electrical.CableDevice
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCablewaysLayoutViews¶
-
SplineSegment.
GetCablewaysLayoutViews
¶ Returns
NXOpen.Routing.Electrical.CablewaysLayoutView
objects from theNXOpen.Routing.ISegment
.Signature
GetCablewaysLayoutViews()
Returns: Array of cableways layout views. Return type: list of NXOpen.Routing.Electrical.CablewaysLayoutView
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCharacteristics¶
-
SplineSegment.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
SplineSegment.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDraftingCurveInfo¶
-
SplineSegment.
GetDraftingCurveInfo
¶ Creates new DraftingCurveInfo object
Signature
GetDraftingCurveInfo()
Returns: New DraftingCurveInfo object. Returns None if the input curve is not a drafting curve :rtype:
NXOpen.Drawings.DraftingCurveInfo
New in version NX10.0.0.
License requirements: None.
GetEndPoints¶
-
SplineSegment.
GetEndPoints
¶ Get the current location of the segment ends in ABS coordinates.
This value is overridden by the coordinates of the end RCPs associated with this segment.
Signature
GetEndPoints()
Returns: a tuple Return type: A tuple consisting of (startPoint, endPoint). startPoint is a NXOpen.Point3d
. Location of end 0 in ABS coordinates endPoint is aNXOpen.Point3d
. Location of end 1 in ABS coordinatesNew in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetEndRcps¶
-
SplineSegment.
GetEndRcps
¶ Return of segment end control points.
The
NXOpen.Routing.ControlPoint
defines an end of a segmentSignature
GetEndRcps()
Returns: a tuple Return type: A tuple consisting of (startRcp, endRcp). startRcp is a NXOpen.Routing.ControlPoint
. RCP defining start of segment endRcp is aNXOpen.Routing.ControlPoint
. RCP defining end of segmentNew in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetGuid¶
-
SplineSegment.
GetGuid
¶ Returns the Globally Unique Identifier (GUID) for this segment.
Signature
GetGuid()
Returns: The GUID for this segment. Return type: str New in version NX8.0.3.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
SplineSegment.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIsEccentricSegment¶
-
SplineSegment.
GetIsEccentricSegment
¶ Is given segment a eccentric segment?
Signature
GetIsEccentricSegment()
Returns: Is segment a eccentric segment? Return type: NXOpen.Routing.Eccentric
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetIsSegmentInterior¶
-
SplineSegment.
GetIsSegmentInterior
¶ Query if a segment is interior to any part
Signature
GetIsSegmentInterior()
Returns: Is segment interior? Return type: NXOpen.Routing.Interior
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetIsTerminalSegment¶
-
SplineSegment.
GetIsTerminalSegment
¶ Is given segment a terminal segment?
Signature
GetIsTerminalSegment()
Returns: Is segment a terminal segment? Return type: NXOpen.Routing.Terminal
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
SplineSegment.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetSegmentAllStocks¶
-
SplineSegment.
GetSegmentAllStocks
¶ Returns
NXOpen.Routing.Stock
as well asNXOpen.Routing.Overstock
objects from theNXOpen.Routing.ISegment
.Signature
GetSegmentAllStocks()
Returns: Array of stocks/overstocks. Return type: list of NXOpen.Routing.Stock
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetSegmentStock¶
-
SplineSegment.
GetSegmentStock
¶ Returns all stocks that directly reference this segment as part of the path defining the stock.
Signature
GetSegmentStock()
Returns: Return type: list of NXOpen.Routing.Stock
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
SplineSegment.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
SplineSegment.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetCharacteristic¶
-
SplineSegment.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (int) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (float) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (str) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristic2¶
-
SplineSegment.
SetCharacteristic2
¶ Overloaded method SetCharacteristic2
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
-------------------------------------
Sets or creates an integer type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (int) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a double type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (float) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a string type type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (str) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
SplineSegment.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristics2()
instead.License requirements: routing_base (“Routing Basic”)
SetCharacteristics2¶
-
SplineSegment.
SetCharacteristics2
¶ Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit part attributes on the stock part. For legacy parts where the attributes are on the stock component, the attributes will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit attributes on the corresponding instance. For legacy parts where the attribute is on the component, the attributes will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create attributes on the object itself.
Signature
SetCharacteristics2(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –NXOpen.Routing.CharacteristicList
having the titles, types and values of Attributes to be setNew in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
SetEndPoints¶
-
SplineSegment.
SetEndPoints
¶ Set the current location of the segment ends in ABS coordinates.
This value is overridden by the coordinates of the end RCPs associated with this segment.
Signature
SetEndPoints(startPoint, endPoint)
Parameters: - startPoint (
NXOpen.Point3d
) – New location of end 0 in ABS coordinates - endPoint (
NXOpen.Point3d
) – New location of end 1 in ABS coordinates
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- startPoint (
SetEndRcps¶
-
SplineSegment.
SetEndRcps
¶ Signature
SetEndRcps(startRcp, endRcp)
Parameters: - startRcp (
NXOpen.Routing.ControlPoint
) – RCP defining start of segment - endRcp (
NXOpen.Routing.ControlPoint
) – RCP defining end of segment
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- startRcp (
SetIsTerminalSegment¶
-
SplineSegment.
SetIsTerminalSegment
¶ Set given segment to be a terminal segment?
Signature
SetIsTerminalSegment(isTerminal)
Parameters: isTerminal ( NXOpen.Routing.Terminal
) – Set as terminal segment?New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetName¶
-
SplineSegment.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSegmentInteriorPart¶
-
SplineSegment.
SetSegmentInteriorPart
¶ Set a segment to be interior to supplied part
Signature
SetSegmentInteriorPart(interiorPart)
Parameters: interiorPart ( NXOpen.Assemblies.Component
) – Part segment interior?New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)