Interior Enumeration¶
-
class
NXOpen.Routing.
Interior
¶ Bases:
object
Option to query if an existing
NXOpen.Routing.ISegment
is interior to anyNXOpen.Part
.Enum Members
Enum Member Enum Member Description NotInteriorToPart Is not interior to any partInteriorToPart Is interior to some part-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-