Eccentric Enumeration¶
-
class
NXOpen.Routing.
Eccentric
¶ Bases:
object
Option to query if an existing
NXOpen.Routing.ISegment
is a eccentric segment.Enum Members
Enum Member Enum Member Description NotEccentricSeg Is not a eccentric segmentEccentricSeg Is a eccentric segment-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-