StockTransitionBuilder Class¶
-
class
NXOpen.Routing.
StockTransitionBuilder
¶ Bases:
NXOpen.Builder
Builder for creating/editing stockTransition.
Create StockTransition: Takes a set of segments and assign characteristics of the selected stock to the segments.
Edit Stock: Takes in the selected stockTransition to edit as input and redefines the stockTransition with the new settings.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateStockTransitionBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
EndProfileOriginCurve | Returns the origin curve of end profile |
EndProfileOriginCurveDirection | Returns or sets the direction of origin curve of end profile |
SegmentCollector | Returns the segment collector |
StartProfileOriginCurve | Returns the origin curve of start profile |
StartProfileOriginCurveDirection | Returns or sets the direction of origin curve of start profile |
StockSettings | Returns or sets the stock settings for stock assignment. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetStockTransitionProperties | |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndProfileOriginCurve¶
-
StockTransitionBuilder.
EndProfileOriginCurve
¶ Returns the origin curve of end profile
-------------------------------------
Getter Method
Signature
EndProfileOriginCurve()
Returns: Return type: NXOpen.SelectCurve
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
EndProfileOriginCurveDirection¶
-
StockTransitionBuilder.
EndProfileOriginCurveDirection
¶ Returns or sets the direction of origin curve of end profile
-------------------------------------
Getter Method
Signature
EndProfileOriginCurveDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
EndProfileOriginCurveDirection(endProfileOriginCurveDirection)
Parameters: endProfileOriginCurveDirection (bool) – New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SegmentCollector¶
-
StockTransitionBuilder.
SegmentCollector
¶ Returns the segment collector
-------------------------------------
Getter Method
Signature
SegmentCollector()
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
StartProfileOriginCurve¶
-
StockTransitionBuilder.
StartProfileOriginCurve
¶ Returns the origin curve of start profile
-------------------------------------
Getter Method
Signature
StartProfileOriginCurve()
Returns: Return type: NXOpen.SelectCurve
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
StartProfileOriginCurveDirection¶
-
StockTransitionBuilder.
StartProfileOriginCurveDirection
¶ Returns or sets the direction of origin curve of start profile
-------------------------------------
Getter Method
Signature
StartProfileOriginCurveDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
StartProfileOriginCurveDirection(startProfileOriginCurveDirection)
Parameters: startProfileOriginCurveDirection (bool) – New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
StockSettings¶
-
StockTransitionBuilder.
StockSettings
¶ Returns or sets the stock settings for stock assignment.
-------------------------------------
Getter Method
Signature
StockSettings()
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
StockSettings(pathStockBuilder)
Parameters: pathStockBuilder ( NXOpen.Routing.PathStockBuilder
) –New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
SetStockTransitionProperties¶
-
StockTransitionBuilder.
SetStockTransitionProperties
¶ Signature
SetStockTransitionProperties()
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Validate¶
-
StockTransitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.