RoutePartDescriptor Class¶
-
class
NXOpen.Routing.
RoutePartDescriptor
¶ Bases:
NXOpen.TaggedObject
Represents a part descriptor chrx.
To create a new instance of this class, use
NXOpen.Routing.RoutePartDescriptorCollection.CreatePartDescriptor()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DescriptorCharxType | Returns or sets the charx type for the part descriptor used by Routing. |
DescriptorSourceType | Returns or sets the descriptor type for the part descriptor used by Routing. |
Expression | Returns or sets the expression for the part descriptor used by Routing. |
Tag | Returns the Tag for this object. |
Title | Returns or sets the title for the part descriptor used by Routing. |
Methods¶
Enumerations¶
RoutePartDescriptorCharxType Enumeration | Charx Type for a NXOpen.Routing.RoutePartDescriptor . |
RoutePartDescriptorSourceType Enumeration | Descriptor Type for a NXOpen.Routing.RoutePartDescriptor . |
Property Detail¶
DescriptorCharxType¶
-
RoutePartDescriptor.
DescriptorCharxType
¶ Returns or sets the charx type for the part descriptor used by Routing.
-------------------------------------
Getter Method
Signature
DescriptorCharxType()
Returns: Return type: NXOpen.Routing.RoutePartDescriptorCharxType
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DescriptorCharxType(type)
Parameters: type ( NXOpen.Routing.RoutePartDescriptorCharxType
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
DescriptorSourceType¶
-
RoutePartDescriptor.
DescriptorSourceType
¶ Returns or sets the descriptor type for the part descriptor used by Routing.
-------------------------------------
Getter Method
Signature
DescriptorSourceType()
Returns: Return type: NXOpen.Routing.RoutePartDescriptorSourceType
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DescriptorSourceType(type)
Parameters: type ( NXOpen.Routing.RoutePartDescriptorSourceType
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Expression¶
-
RoutePartDescriptor.
Expression
¶ Returns or sets the expression for the part descriptor used by Routing.
-------------------------------------
Getter Method
Signature
Expression()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Expression(expression)
Parameters: expression (str) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Title¶
-
RoutePartDescriptor.
Title
¶ Returns or sets the title for the part descriptor used by Routing.
-------------------------------------
Getter Method
Signature
Title()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Title(title)
Parameters: title (str) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)