RoutePartDescriptorCharxType Enumeration

NXOpen.Routing.RoutePartDescriptor.CharxType is an alias for NXOpen.Routing.RoutePartDescriptorCharxType

class NXOpen.Routing.RoutePartDescriptorCharxType

Bases: object

Charx Type for a NXOpen.Routing.RoutePartDescriptor.

Enum Members

Enum Member Enum Member Description
Int  
Real  
Sting  
Any  
Ref  
AnyRef  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.