QuickPathBuilder Class¶
-
class
NXOpen.Routing.
QuickPathBuilder
¶ Bases:
NXOpen.Builder
Builder for creating a path between user selected points.
After invoking the commit method, invoke the
NXOpen.Routing.QuickPathBuilder.PathErrors()
method to find out which sections between points contained errors.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateQuickPathBuilder()
Default values.
Property Value PathSettings.LockToSelectedObject True New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
PathErrors | Returns the errors associated with this path. |
PathSettings | Returns the linear path settings for this path. |
PointList | Returns the list of path points. |
RouteSegment | Returns the routing segment managed by the builder, if it exists. |
StockSettings | Returns the stock settings for this path. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetListOfPointsToDraw | Save a point or extension point to the list of all points to draw on the screen. |
SetListOfPointsToDrawCount | Set the number of elements in the list of all points to draw on the screen. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
PathErrors¶
-
QuickPathBuilder.
PathErrors
¶ Returns the errors associated with this path.
The list will be None if the commit method has not been invoked yet.
-------------------------------------
Getter Method
Signature
PathErrors()
Returns: The list of errors. Return type: NXOpen.ErrorList
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
PathSettings¶
-
QuickPathBuilder.
PathSettings
¶ Returns the linear path settings for this path.
-------------------------------------
Getter Method
Signature
PathSettings()
Returns: Return type: NXOpen.Routing.LinearPathSettings
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
PointList¶
-
QuickPathBuilder.
PointList
¶ Returns the list of path points.
-------------------------------------
Getter Method
Signature
PointList()
Returns: Return type: NXOpen.PointList
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RouteSegment¶
-
QuickPathBuilder.
RouteSegment
¶ Returns the routing segment managed by the builder, if it exists.
-------------------------------------
Getter Method
Signature
RouteSegment()
Returns: Visible Routing BCurve Segment Return type: NXOpen.Curve
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
StockSettings¶
-
QuickPathBuilder.
StockSettings
¶ Returns the stock settings for this path.
-------------------------------------
Getter Method
Signature
StockSettings()
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
SetListOfPointsToDraw¶
-
QuickPathBuilder.
SetListOfPointsToDraw
¶ Save a point or extension point to the list of all points to draw on the screen.
Signature
SetListOfPointsToDraw(index, point)
Parameters: - index (int) – The index in the list of points to draw.
- point (
NXOpen.Point3d
) – Point representing the position.
New in version NX8.5.3.
License requirements: routing_base (“Routing Basic”)
SetListOfPointsToDrawCount¶
-
QuickPathBuilder.
SetListOfPointsToDrawCount
¶ Set the number of elements in the list of all points to draw on the screen.
Signature
SetListOfPointsToDrawCount(count)
Parameters: count (int) – The number of points in list. New in version NX10.0.2.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
QuickPathBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.