LinearPathSettings Class¶
-
class
NXOpen.Routing.
LinearPathSettings
¶ Bases:
NXOpen.Builder
Helper object used the by
Routing.LinearPathBuilder
builder.Determines various settings to be applied when the path is created.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateLinearPathSettings()
Default values.
Property Value LockToSelectedObject True New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AllowCutElbow | Returns or sets a flag indicating whether or not to allow cut elbow placement |
AssignDefaultCorner | Returns or sets the preference to assign the current default corner to new segments. |
AssignDefaultElbow | Returns or sets the preference to find and assign a default elbow to new segments. |
LockAngle | Returns or sets the preference to determine if the angle between segments should be constrained. |
LockLength | Returns or sets the preference to determine if the length of new segments should be constrained. |
LockToSelectedObject | Returns or sets the preference to determine if the new segments and control points should be constrained to the objects selected by the user. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllowCutElbow¶
-
LinearPathSettings.
AllowCutElbow
¶ Returns or sets a flag indicating whether or not to allow cut elbow placement
-------------------------------------
Getter Method
Signature
AllowCutElbow()
Returns: Return type: bool New in version NX8.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)
-------------------------------------
Setter Method
Signature
AllowCutElbow(assign)
Parameters: assign (bool) – New in version NX8.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)
AssignDefaultCorner¶
-
LinearPathSettings.
AssignDefaultCorner
¶ Returns or sets the preference to assign the current default corner to new segments.
-------------------------------------
Getter Method
Signature
AssignDefaultCorner()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AssignDefaultCorner(assign)
Parameters: assign (bool) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
AssignDefaultElbow¶
-
LinearPathSettings.
AssignDefaultElbow
¶ Returns or sets the preference to find and assign a default elbow to new segments.
-------------------------------------
Getter Method
Signature
AssignDefaultElbow()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AssignDefaultElbow(assign)
Parameters: assign (bool) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
LockAngle¶
-
LinearPathSettings.
LockAngle
¶ Returns or sets the preference to determine if the angle between segments should be constrained.
-------------------------------------
Getter Method
Signature
LockAngle()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
LockAngle(lock)
Parameters: lock (bool) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
LockLength¶
-
LinearPathSettings.
LockLength
¶ Returns or sets the preference to determine if the length of new segments should be constrained.
-------------------------------------
Getter Method
Signature
LockLength()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
LockLength(lock)
Parameters: lock (bool) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
LockToSelectedObject¶
-
LinearPathSettings.
LockToSelectedObject
¶ Returns or sets the preference to determine if the new segments and control points should be constrained to the objects selected by the user.
-------------------------------------
Getter Method
Signature
LockToSelectedObject()
Returns: Return type: bool New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
LockToSelectedObject(lock)
Parameters: lock (bool) – New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
LinearPathSettings.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.