SegmentManagerSubdivideSpacing Enumeration¶
NXOpen.Routing.SegmentManager.SubdivideSpacing is an alias for NXOpen.Routing.SegmentManagerSubdivideSpacing
-
class
NXOpen.Routing.
SegmentManagerSubdivideSpacing
¶ Bases:
object
Specifies spacing option for subdivide segment.
Enum Members
Enum Member Enum Member Description ScreenPoint Screen PointEqualArcLength Equal Arc LengthEqualParameter Equal ParameterIncrementalArcLength Incremental Arc LengthGeometricRatio Geometric Progression RatioChordalTolerance Chordal ToleranceNumberOfOptions Number of Options-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-