PortConnectionCollectionPortsStatus Enumeration¶
NXOpen.Routing.PortConnectionCollection.PortsStatus is an alias for NXOpen.Routing.PortConnectionCollectionPortsStatus
-
class
NXOpen.Routing.
PortConnectionCollectionPortsStatus
¶ Bases:
object
Option to check if two ports can be connected by creating a
NXOpen.Routing.PortConnection
object.Enum Members
- using Port Connection object. “
- “CannotConnect”, ” The Ports cannot be connected
using Port Connection object. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.