OverstockBuilderApplicationType Enumeration¶
NXOpen.Routing.OverstockBuilder.ApplicationType is an alias for NXOpen.Routing.OverstockBuilderApplicationType
-
class
NXOpen.Routing.
OverstockBuilderApplicationType
¶ Bases:
object
The overstock application type.
This defines the way in which to create piggyback segment for overstock.
Enum Members
Enum Member Enum Member Description EntireSegments Entire SegmentsInterval IntervalPointToPoint Point To PointPointAndLength Point And Length-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-