ReuseLibraryPartType Enumeration¶
NXOpen.Routing.ReuseLibrary.PartType is an alias for NXOpen.Routing.ReuseLibraryPartType
-
class
NXOpen.Routing.
ReuseLibraryPartType
¶ Bases:
object
Represents the part type.
Enum Members
Enum Member Enum Member Description Gasket Gasket Post Placement TypeBolt Bolt Post Placement TypeStud Stud Post Placement TypeNut Nut Post Placement TypeWasher Washer Post Placement TypeWeldring Weld Ring Post Placement TypeRingjoint Ring Joint Post Placement TypeUnknown Unknown Type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-