DesignRuleViolationCollectionMode Enumeration¶
NXOpen.Routing.DesignRuleViolationCollection.Mode is an alias for NXOpen.Routing.DesignRuleViolationCollectionMode
-
class
NXOpen.Routing.
DesignRuleViolationCollectionMode
¶ Bases:
object
Design Rule Mode
Enum Members
Use LogConcurrent method on
NXOpen.Routing.RouteManager
to concurrently logged objects and GetConcurrent method to get all the concurrent objects ““Interactive”, ” Execute design rules during next interactive check ” “Batch”, ” Executes design rules in a batch process “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-