TransformPathBuilderTransformOption Enumeration¶
NXOpen.Routing.TransformPathBuilder.TransformOption is an alias for NXOpen.Routing.TransformPathBuilderTransformOption
-
class
NXOpen.Routing.
TransformPathBuilderTransformOption
¶ Bases:
object
Tranform operation to perform.
Enum Members
Enum Member Enum Member Description MoveOriginal Move the selected entities.CopyOriginal Copy the selected entities.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-