RouteManagerImportMode Enumeration¶
NXOpen.Routing.RouteManager.ImportMode is an alias for NXOpen.Routing.RouteManagerImportMode
-
class
NXOpen.Routing.
RouteManagerImportMode
¶ Bases:
object
Route List import modes
The following tables describes the effects of the various modes depending on the type (XML, HRN, CMP) of import. <code> ++————–+—————+—————–+ +————+————++ Deletes | Replaces data | Preserves | | | Import || unmatched | in matching | existing | | ImportMode | File Type || elements | elements | connectors | +============+============++==============+===============+=================+ | Update | XML || Yes | Yes | No | | | Legacy CMP || No | Yes | Yes | | | Legacy HRN || Yes(1) | Yes(2) | Yes | +————+————++————–+—————+—————–+ | Merge | XML || No | Yes | Yes | | | Legacy CMP || No | Yes | Yes | | | Legacy HRN || No | Yes(2) | Yes | +————+————++————–+—————+—————–+ | Append | XML || No | No | Yes | | | Legacy CMP || No | No | Yes | | | Legacy HRN || No | No | Yes | +————+————++————–+—————+—————–+
++————–+—————+—————–+——————+ +————+————++ May add new | May add new | May create | May create | | | Import || connectors | connections | duplicate | duplicate | | ImportMode | File Type || | | connector names | connection names | +============+============++==============+===============+=================+==================+ | Update | XML || Yes | Yes | Yes(3) | Yes(3) | | | Legacy CMP || Yes | No | No | No | | | Legacy HRN || Yes | Yes | No | No | +————+————++————–+—————+—————–+——————+ | Merge | XML || Yes | Yes | Yes(3) | Yes(3) | | | Legacy CMP || Yes | No | No | No | | | Legacy HRN || Yes | Yes | No | No | +————+————++————–+—————+—————–+——————+ | Append | XML || Yes | Yes | Yes | Yes | | | Legacy CMP || Yes | No | Yes | No | | | Legacy HRN || Yes | Yes | No | Yes | +————+————++————–+—————+—————–+——————+
++————–+—————+—————–+ || Maintains | Maintains | Elements | || assignment | routing | matching | +————+————++ information | information | criterion | | | Import || for matching | for matching | | | ImportMode | File Type || connectors | connections | | +============+============++==============+===============+=================+ | Update | XML || Yes | Yes | GUID | | | Legacy CMP || Yes | Yes | Names(4) | | | Legacy HRN || Yes | Yes | Names(4) | +————+————++————–+—————+—————–+ | Merge | XML || Yes | Yes | GUID | | | Legacy CMP || Yes | Yes | Names(4) | | | Legacy HRN || Yes | Yes | Names(4) | +————+————++————–+—————+—————–+ | Append | XML || No | No | N/A | | | Legacy CMP || No | No | N/A | | | Legacy HRN || No | No | N/A | +————+————++————–+—————+—————–+ </code>
- Connection list data only (no connectors)
- Connector data is not updated
- Since matches are made using GUIDs only, no attempt is made to prevent duplicate names
- Technically, legacy import does check GUIDs as well but using GUID is not practical with legacy import
Enum Members
Enum Member Enum Member Description Update Update existing objects with data from the imported objects.Merge Update existing objects with data from the imported objects.Append Create the imported objects as new objects.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.