ControlPointCollectionFoundExisting Enumeration¶
NXOpen.Routing.ControlPointCollection.FoundExisting is an alias for NXOpen.Routing.ControlPointCollectionFoundExisting
-
class
NXOpen.Routing.
ControlPointCollectionFoundExisting
¶ Bases:
object
Whether
NXOpen.Routing.ControlPoint
returned from the creator methods was an existingNXOpen.Routing.ControlPoint
or a newNXOpen.Routing.ControlPoint
.Enum Members
Enum Member Enum Member Description BrandNew Object is a new object.Existing Object existed already.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-