IntegrateRunsBuilderButton Enumeration¶
NXOpen.Routing.IntegrateRunsBuilder.Button is an alias for NXOpen.Routing.IntegrateRunsBuilderButton
-
class
NXOpen.Routing.
IntegrateRunsBuilderButton
¶ Bases:
object
Enums to distinguish callback’s for from/to/member Item buttons
Enum Members
Enum Member Enum Member Description FromItems Set as FromItem for selected node in tree listToItems Set as ToItem for selected node in tree listMemberItems Set as MemberItem for selected node in tree listUnknown unknown button ID-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-