UserDefined Enumeration¶
-
class
NXOpen.Routing.
UserDefined
¶ Bases:
object
Option to indicate if an existing
NXOpen.Routing.LineSegment
,NXOpen.Routing.ArcSegment
orNXOpen.Routing.SplineSegment
is user defined.Enum Members
- System manages simplification and some update behavior. “
- “UserDefined”, ” User defined generated segment. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.