FormboardFrameCollection Class¶
-
class
NXOpen.Routing.
FormboardFrameCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.FormboardFrame
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateFormboardFrameByRectangle | Creates a NXOpen.Routing.FormboardFrame object using a rectangle defined by a NXOpen.Point object and two NXOpen.Scalar objects that represent the height and width. |
ImportPattern | Creates a NXOpen.Routing.FormboardFrame object by importing formboard frame pattern @return returning new frame |
Method Detail¶
CreateFormboardFrameByRectangle¶
-
FormboardFrameCollection.
CreateFormboardFrameByRectangle
¶ Creates a
NXOpen.Routing.FormboardFrame
object using a rectangle defined by aNXOpen.Point
object and twoNXOpen.Scalar
objects that represent the height and width.Signature
CreateFormboardFrameByRectangle(point, height, width)
Parameters: - point (
NXOpen.Point
) – Lower left corner - height (
NXOpen.Scalar
) – - width (
NXOpen.Scalar
) –
Returns: Return type: New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
- point (
ImportPattern¶
-
FormboardFrameCollection.
ImportPattern
¶ Creates a
NXOpen.Routing.FormboardFrame
object by importing formboard frame patternSignature
ImportPattern(filename, type, frameName)
Parameters: - filename (str) – Filename of the file to be imported
- type (int) – Type of file imported
- frameName (str) – new name of frame
Returns: a tuple
Return type: A tuple consisting of (newFrame, group).
newFrame is a
NXOpen.Routing.FormboardFrame
. returning new frame group is aNXOpen.DisplayableObject
. returning the geometry of imported file .. versionadded:: NX5.0.0License requirements: routing_harness (“Routing Harness”)